STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Linux installation error

d64.deb'Note, selecting 'st-stlink-udev-rules' instead of './st-stlink-udev-rules-1.0.3-2-linux-all.deb'Note, selecting 'st-stm32cubeide-1.15.1' instead of './st-stm32cubeide-1.15.1-21094-20240412-1041_amd64.deb'Note, selecting 'segger-jlink-udev-rul...

shri1 by Associate II
  • 6621 Views
  • 13 replies
  • 4 kudos

Resolved! Unit tests in STM32CubeIDE

Currently I'm developing within the STM32CubeIDE for an STM32F373CC.I use the main.c as entry point into a wrapper and program all of the rest in C++. I generally try to keep any HAL code outside of simple classes that can be unit tested easily. Idea...

0693W000004I6ydQAC.png
MMich.2 by Associate II
  • 19976 Views
  • 11 replies
  • 8 kudos

Resolved! Code Generation Bug STM32U5 with VDDA

Hello! I believe I found a code generation bug. I am currently using IDE version 1.16.1.By default, when enabling ADC with an STM32U5, HAL_MSPInit() has the line: HAL_PWREx_EnableVddA() which is necessary to have a positive reference for the ADCs (th...

rgangwan by Associate
  • 1972 Views
  • 2 replies
  • 3 kudos

Generating code for HTTPD in NUCLEO-H745ZI Board

Hi Team,"I am trying to configure an HTTP server on the Nucleo-H745ZIT6 board, which has two Cortex cores. I am using Cortex-M7 for this. After enabling HTTP in middleware inside LwIP, and generating the code, LwIP is placed inside the Cortex-M7 fold...

ggowd.1 by Associate III
  • 8296 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.