2023-08-13 1:44 PM
Hello,
I'm trying to run an example in CubeIDE 1.13.1, but receive the following error. Strangely, executing that binary from the command line in terminal does work...
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_932A7A.log
ST-LINK SN : 066EFF525282494867242444
ST-LINK FW : V2J42M27
Board : NUCLEO-F446RE
Voltage : 3.25V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x421
Revision ID : Rev A
Device name : STM32F446xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_hAMQNL.srec
File : ST-LINK_GDB_server_hAMQNL.srec
Size : 398.77 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_2.1.0.202305091550/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Shutting down...
Exit.
Solved! Go to Solution.
2023-08-13 6:10 PM
So this actually ended up being that the board was previously used and returned to Mouser...
All write protect bits were set... SPRMOD was also changed from the default. Opening up STM32Prog and resetting things from there worked and the board can now be flashed.
2023-08-13 5:14 PM
Try version 1.12.1
2023-08-13 6:10 PM
So this actually ended up being that the board was previously used and returned to Mouser...
All write protect bits were set... SPRMOD was also changed from the default. Opening up STM32Prog and resetting things from there worked and the board can now be flashed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.