2024-09-19 5:05 AM - edited 2024-09-19 5:06 AM
My setup is macOS 15.0 Sequoia
STM32CubeIDE 1.16.1
STLink-Server v2.1.1
When trying to program or debug a device the following error is shown:
Even after re-installing ST-Link server
I have rebooted and re-installed ST-Link Server, but the issue persists.
It's not a show stopper as I can use STM32CubeProgrammer to program the device, on the same machine.
Solved! Go to Solution.
2024-09-25 2:02 AM - edited 2024-09-25 2:03 AM
@pdmazariegos Thanks for the link to that solution on stackoverflow.
I find that it does indeed work. It's a better workaround than the one I came up with!
Hopefully the dev's at ST will be able to get to the bottom of it and push out a compatibiliy release in the near future. I have to keep my macOS up to date for other reasons, so I had no choice but to update to macOS 15.0
@mƎALLEm Do you know if ST run a beta programme? I'd be happy to help with beta testing.
*edit* Spelling.
2024-09-28 1:36 AM
another one with the same problem:
2024-11-05
1:40 AM
- last edited on
2024-11-05
2:47 AM
by
Maxime_MARCHETT
2025-04-07 2:54 AM
I am getting 'source not found' in MAC OS 15 on an M2 PRO
2025-04-07 3:02 AM
@rclar.6 What version of STM32CubeIDE are you running?
2025-04-07 3:24 AM
@rclar.6 Is this actually related to the original Topic from 2024, "BUG: STM32CubeIDE Won't connect to ST-LINK v2 debugger on macOS 15.0" ?
That was marked as solved, with the solution being: macOS15 is not supported yet.
Have you confirmed that MacOS 15 should now be supported?
2025-04-07 3:33 AM - edited 2025-04-07 3:34 AM
1.1.18 I think. I downloaded the latest version (from 1.1.14) in the hope it would fix it.
2025-04-07 3:37 AM
So does its readme claim that MacOS 15 should now be supported?
2025-04-07 3:38 AM
OK. I was too hasty to upgrade. hopefully a newer version will fix this soon.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.