STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Import and Export

I am fairly new to programming. So I have STM32CUBEide at work and at home. If find it extrodnarilly difficult to work on something at the office and then take it home or in reverse. I have tried exporting, importing, importing from the file system a...

Resolved! Updating cube ide manually

I have internet access at my office only through a virtual machine.I'm facing an issue with updating Cube-IDE. Currently, I'm using version 1.11.0 and I want to manually update it to version 1.13.1.I've downloaded the executable file for version 1.13...

version.PNG
Pshar.2 by Associate
  • 6763 Views
  • 2 replies
  • 0 kudos

Can't set breakpoint on CM4 in two-core setup

We've got a STM32H747IGT6 which is the two-core version (one M4, one M7).  I've got GDB servers running on ports 61238 (CM4) and 61234 (CM7) and then running two instances of GDB (one for each server).  GDB says it's happily connected, and I can load...

STM Import Export Project

Hi,I am trying to export (and then import) a project on STMIDE from one computer to another but it's been not so straight forward. Hoping somebody can point me to the right direction or a step by step on how this is properly done. For context, when I...

od805 by Associate III
  • 5244 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.