STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Debugging issues with STM32CubeIDE / STM32F030F4Px

I am having debugging issues with STM32CubeIDE. the processor is STM32F030F4Px and I am using a knock off ST-Link V2. It seem that no matter what I configure I get the same error. There also is a check GDB server version error in the IDE window. Open...

DHirs.2 by Associate
  • 5672 Views
  • 5 replies
  • 0 kudos

SPI GPIO control - AFCNTR bit with LL API

When using SPI LL API on STM32H7, we want to use the CFG2[AFCNTR] bit. When “Master Keep IO option”  is used in the IDE, Cube does not generate the LL_SPI_EnableGPIOControl() function call so that the bit remains unset. This has then has to be called...

Resolved! NUCLEO-H7S3L8 failed to execute MI command

Hello,I bought a Nucleo-H7S3L8 and I'm trying to build and execute the XIP_Template and I'm following the official guide.at first I built the Appli project and I choosed the first debug option and got the following error.to solve it I found a post in...

Screenshot 2025-07-15 at 14.26.49.png Screenshot 2025-07-15 at 14.28.17.png Screenshot 2025-07-15 at 15.03.58.png Screenshot 2025-07-15 at 16.08.09.png
oalselwi by Associate II
  • 915 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.