STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F030F4 with STM32Cube tools

Hi I used STM32CubeMX to create a new project for STM32F030F4 + STM32CubeIDE.The project was created, but when I compile, all the data by default is mapped to address 0x00008000, just after the valid range of the flash mirror. How strange...Problem o...

SSkje.1 by Associate II
  • 6011 Views
  • 12 replies
  • 0 kudos

Problems copying SWV log

I'm trying to copy data from the SWV Trace Log but when I try to copy over 1000 lines, Ctl-C brings up a "save as" dialog, and the data that are saved are corrupted with duplicated lines. It looks like there is a rounding error on the export so that ...

tjcrone by Associate
  • 2718 Views
  • 5 replies
  • 0 kudos

Any advantages of Segger J-Link debuggers with STM32CubeIDE?

I have been developing boards with STM32G07x and STM32G07x G47x using ST-Link V2. I thought I would buy a better debug probe allowing more breakpoints and as a future investment in my development activities.I am considering Segger J-Link Base, Plus ...

SSton.1 by Associate III
  • 3301 Views
  • 2 replies
  • 0 kudos

I ordered Nucleo-L4A6ZG few days ago, but CubeIDE 1.4 doesn't support Nucleo-L4A6ZG. How can I develop my board?

I ordered Nucleo-L4A6ZG few days ago, but CubeIDE 1.4 doesn't support Nucleo-L4A6ZG. ​I don't have enough time to wait for a new order, I have to develop my board until next week. ​Is there any solution to develop Nucleo-L4A6ZG board with STM32cubeID...

SLEE.5 by Associate
  • 1390 Views
  • 3 replies
  • 0 kudos

Can't debug NUCLEO-F746ZG in STM32CubeIDE

Hi AllI can drag and drop a binary file to the NUCLEO-F746ZG via its mbed hard drive that appears when the board is connected to the PC and the program runs.I can also try to debug from STM32CubeIDE and it successfully programs and verifies the code ...

hpipon957 by Associate III
  • 4629 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.