2020-07-23 5:20 AM
I'm trying to copy data from the SWV Trace Log but when I try to copy over 1000 lines, Ctl-C brings up a "save as" dialog, and the data that are saved are corrupted with duplicated lines. It looks like there is a rounding error on the export so that lines are duplicated. Is there a CubeIDE setting that could fix this issue? Why does Ctl-C bring up "save as"? Any advice would help greatly. Thank you!
2020-07-23 8:18 AM
Copy and paste for SWV logs as well as the SWV Exception Timeline Graph seems to work fine in TrueStudio 9.3.0. I will be going back to TrueStudio until the numerous SWV bugs are worked out in CubeIDE. In the meantime, if anyone finds a solution to these issues please let us know. Cheers.
2020-07-23 1:54 PM
Got info such is known issue. Maybe fixed soon.
2020-07-24 1:01 AM
This should be fixed in the new release of CubeIDE which should be coming in the next few days, hopefully early next week. If it's still a problem after the release please let me know.
2020-07-24 1:12 AM
Good news! Thanks for update.
2020-07-28 11:47 AM
Works for me now based on fresh STM32CubeIDE 1.4.0 release.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.