STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't include new folders in STM23CubeIDE project?

I've created a new folder inside the User directory where main.c is, but when adding the path in the includes list it still can't find it?I've done it exactly the same way as the other two but for some reason it's just not working now.If I move the f...

JWood by Associate II
  • 2555 Views
  • 3 replies
  • 0 kudos

Ask for errors related to 'Mon64.dll'

Hello, colleaguesI have a problem in building the project.I installed STM32CubeIDE (Ver. 1.4.2) and generated code successfully.(I applied only the clock configuration and RCC setup)When I tried to build the project, however, I faced several errors l...

0693W000003Pi28QAC.jpg
HKim.9 by Associate
  • 1017 Views
  • 0 replies
  • 0 kudos

is available cmsis-dsp on cubeIDE version 1.4.0?

in last version of cubeIDE it was possible to include cmsis-DSP only selecting from package selector ARM and then only choose cmsis dsp, but i cannot see in this tab in cudeIDE 1.4.2, this feature has been removed in this current version ? and if thi...

What is Command to Generate Binary for external flash. I want to add command in STM32CubeIDE Project->Properties->C/C++ build-> Settings->BuildStep->Post Build Step->Commnds:

We are Planning to Use STM32F7508-DK board for our Application. As I go through Datasheet of it. It is mention that 64 KB for internal flash. But I am very sure that my application required more than 64 KB. PFA first Question: As I can see my project...

0693W000003Pc72QAC.png 0693W000003Pc6xQAC.png

[BUG] The IDE version has not changed after being updated (LINUX)

After installing update 1.4.1 the splash field showing 1.4.0 has not changed.It continues even after opening and closing several times.In Windows I noticed that this occurs only once, then the number is corrected.(I am reporting this, because if a si...

by Not applicable
  • 2859 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.