STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE hangs at end of build

I have an STM32CubeIDE project I've been working on for several months. In 1.4.x, it will hang at the end of the build. It'll report "0 errors, 0 warnings", but the status window doesn't go away and it still says "Building Project". I have to force q...

Resolved! Program a new L152 chip (in STM32CubeIDE)

HelloI did some basic testing to set up, write code and program the STM32 F103 (bluepill) with the STM32CubeIDE and everything worked fine!In a project I would like to design my own PCB and use the L152C8T6 chip. So I purchased some new chips from Di...

0693W000004JDhbQAG.jpg 0693W000004JDzpQAG.jpg 0693W000004JE2eQAG.jpg
NiJo by Associate
  • 1768 Views
  • 2 replies
  • 0 kudos

Error on entering debug mode

Hi everyone,After using IAR and Keil for several years, i decided to try STM32IDE.I generated an initialization code using STM32cubemx, and used STM32IDE for compiling and programming my STM32 board. However, it generated an error and was not able to...

AJafa.2 by Associate II
  • 4678 Views
  • 7 replies
  • 0 kudos

Resolved! Why no example code for STM32F0Discovery?

The STM32F0Discovery board comes with accompanying example source code, traditionally. However, now, the relevant download page advises that this is all provided by STM32Cube, but it is not. There is NO example code in the STM32CubeMX / IDE for this ...

Resolved! How to change memory areas in CubeIDE?

If I need to change memory areas in project (for example for Read-only memory I need 0x8080000 start, 0x40000 size), how can I do in in CubeIDE ? (addition) I have found Build analyzer, but the fields are not changeable, only view.

STM32F4 training ?

Hi, I have found 12 videos on Youtube for the STM32CubeIDE - basics but these require the use of a Nucleo-G071RB board.I have an STM32F407VGT6 based Discovery board. Does ST provide any training materials for the STM32F407 line of MCUs utilising the ...

I have a Nucleo-F030R8 and a STM32 Discovery MB1034B which has an STM32F051R8T6 which I am programming from the STM32CubeIDE environment. They don't function the same in Device Manager definitions of capabilities.

Under the Device Manager "Universal Serial Bus devices" \tThe Nucleo board is identified as "ST-Link Debug" whereas the Discovery board is identified as "STM32 STLink" though they show the same driver. Further, the Nucleo creates a "COM" device whic...

RSimp by Associate II
  • 1829 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.