STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE generates high CPU load (Win7)

Hi,I installed STM32CubeIDE (Version: 1.1.0, Build: 4551_20191014-1140 (UTC)) on my laptop (Win7, 64bit). The installation path is "C:\tools\ST\STM32CubeIDE_1.1.0\STM32CubeIDE" As soon as I start the IDE the CPU load on my laptop the CPU load goes up...

headless-build JVM terminated

First of all, I want to ask whether my use case is achievable with headless-build:I want to build my project (with frequently changing files and directories) from terminal[In Terminal]: [Project]/Release: make -j12 allWhen I change some source files ...

S_L by Associate
  • 1326 Views
  • 0 replies
  • 0 kudos

Update Site issue on STM32CubeIDE

Hello support team ,i have tried to Update Stm32CubeIDE on update sitehttp://sw-center.st.com/stm32cubeide/updatesite1i have a systematic issueAn error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=or...

I cannot add the ~ character in C or C ++ code editor.

Hello.I am having a problem with the code editor. Under Windows 10 (French), I cannot add the ~ character in C or C ++ code. My only solution is to copy paste this symbol which is displayed in all the other code editors (VS, VSC, ...). I am using cub...

FFRAN.1 by Associate II
  • 1824 Views
  • 3 replies
  • 0 kudos

The UART logs can't be shown on putty correctly

Hi,​I'm a newbie of ST chipset, and just got the STM3241G-EVAL board recently. When I'm trying the example code related to UART, "UART_Hypertermial_it", which can be downloaded with STM32CubeIDE, unfortunately the output from UART can't be shown corr...

XLei.1 by Associate II
  • 969 Views
  • 0 replies
  • 0 kudos

Removal of unused code from project

Hi All,I'm putting together a project that will use the XCube Cellular and Azure Expansion pack.I'm sure there are >100 files that are not used by my project in the above expansion packs.How can I easily determine and remove unwanted files?Thanks,Ne...

NW27 by Associate III
  • 1054 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.