STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

stm32cubeide code error

I tried running the first program, but this error occurred. I haven't done any coding, but I don't know why this error occurs.

0693W000004J3LLQA0.png

Can I use preprocessor commands in linker script and how ?

Hey,Is it possible to use preprocessor commands in linker script file (***.ld) and how it can be done if possible. I want to have diffrent memory definitions depending on the macro. I tried this but it's not working:/* Memories definition */ MEMORY {...

JureL by Senior
  • 6838 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE update 1.4.2 cannot be found on 1.4.0

OS: openSUSE LinuxTrying to update from 1.4.0 to 1.4.2 by clicking Help->Check for updatesResult: "No updates found. Configure available software sites to reach more content."STM32CubeIDE Releases is enabled and when I reloaded it, I saw that it does...

VNorr.1 by Associate
  • 2142 Views
  • 3 replies
  • 0 kudos

I have a problem with the STM32CubeIDE, it consumtion a lot of memory ram. In the task manager it open many conhost.exe process (i attach an imagen). Can you know how avoid open many conhost?. (sorry for my english)

I've seen that when I compile the code all the conhost.exe processes are delete but after that, the conhost begin to open automatically like in the attach imagen.

VRodr by Associate II
  • 7713 Views
  • 7 replies
  • 0 kudos

How do I use the STM32CubeIDE?

I have just downloaded the STM32 IDE, and I find it very complicated to use it. I am using a bare MCU, no dev board, hence I am using the STLink-V2 to program the MCU. I want some help on how to write my program to blink an led and set up the STLink-...

Sashvat by Associate II
  • 2055 Views
  • 3 replies
  • 0 kudos

How to adapt "LwIP_HTTP_Server_Netconn_RTOS" example from NUCLEO-F429ZI evaluation board to an application with STM32F429VET6 microcontroller?

I am trying to adapt "LwIP_HTTP_Server_Netconn_RTOS" example from NUCLEO-F429ZI to a new project based on STM32F429VET6 microcontroller with STM32CubeIDE, but the connection is not accepted when 'netconn_accept()' function is executed, as I have test...

Ml.1 by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

Example project STM32H747I-DISCO with STM32CubeIDE and STemWIN

Hello, I'm struggling to get an example project running for the STM32H747I-DISCO board within SMT32CubeIDE together with STemWIN. I only want to show simple text and values on the display, updating once a second. I tried to import existing projects...

KR51K by Associate III
  • 876 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.