STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hi guys, unfortunately, I did something that I can not spot in my project and it is not compiling anymore. cubmixIDE is saying that: "undefined reference to `HAL_UART_Transmit'" anytime I'm using `HAL_UART_Transmit'.

as people told me, i looked on "makefile" vs last version "makefile" to see any change but i couldnt spot one.I did all necessary "#incuded" on top of the class.I'v attached the problematic part:#include "main.h" #include <string.h> #include <stdboo...

Gbasi.1 by Associate II
  • 1714 Views
  • 3 replies
  • 0 kudos

Workaround for GCC LTO Bug

Unfortunately there is a bug regarding the LTO option since GCC 7 until at least GCC 9: https://bugs.launchpad.net/gcc-arm-embedded/+bug/1747966Can you please consider applying the workaround described there?I.e. in the generated Makefile the startup...

jirre.1 by Associate II
  • 2073 Views
  • 0 replies
  • 0 kudos

Resolved! Using the projects examples.

Hi all,I'm triyng to learn about using the example projects inside the repository folders.For example, I have a STM32F429i-discovery board and I want to load an example:../STM32Cube/Repository/STM32Cube_FW_F4_V1.25.1/Projects/STM32F429I-Discovery/Exa...

JAlca by Senior
  • 1579 Views
  • 2 replies
  • 0 kudos

STM32H755 - Setting STM32CubeIDE for dual-debug

Hi,I'm having some issues with setting up the IDE for dual-debugging so I can access both the M7 and M4 core in the same IDE.I'm using STLink V3Set for debugging and GDB (I could not get the OCD setup working at all).I have tried going through the st...

TOlli by Senior
  • 2487 Views
  • 2 replies
  • 0 kudos

Resolved! New Project fails, what am I missing?

Have installed STM32CubeIDE on my Debian Linux system.Following the QuickStart Guide, I try: File > New > STM32 Projectand it thinks about it and the gives me:-What did I forget to do and where does it tell me to do it?

0693W0000059g6TQAQ.png
PJR42 by Associate II
  • 3644 Views
  • 7 replies
  • 0 kudos

C++ Startup file

I would like the interrupt handlers to be written in the C ++ style, that is, they are static classes, but there is practically no information on the Internet about where to get a C ++ startup file or how to make it yourself. Has anyone encountered s...

AKlep.1 by Associate II
  • 1985 Views
  • 2 replies
  • 0 kudos

arduino shiftIn function to STM32CubeIDE

I made a test code in arduino to read SSI. How can I make the shiftin function work correctly in the stm32 controllers? . In the stm32cubeIDE I can't manage to make it work like in the arduino ide.In the shiftin function the variables: data_pin, cloc...

YTimm.1 by Associate II
  • 1932 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.