STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to generate C++ based project from STM32 Cube IDE v1.4.0

Hi There,I want to generate a project template for STM32F103 based mcu, but the template/project should be C++ based not C based. I tried to mark C++ while creating a new project but still the end result was c based project only. main.c was created i...

DChan.5 by Associate
  • 1695 Views
  • 2 replies
  • 0 kudos

How to use stlink-server?

I've tried to use the stlink-server from here (in my understanding, it's a GDB server). And no success with gcc-arm-none-eabi-9-2020-q2-update toolchain: when I'm trying to target connect localhost:7184I have the following debug output from the stlin...

SDomb by Associate
  • 2088 Views
  • 2 replies
  • 0 kudos

Resolved! Issues with running FatFs_eMMC_Standalone - STM32CubeIDE

I just received an STM32L4P5 Discovery board to evaluate eMMC for the STM32L4. In the firmware package for the STM32L4 there is an example project, "FatFs_eMMC_Standalone". I have built the example, however, when I try to run it the application halts...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.