STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Code changes not being used in debug mode

Hi all, I am very new to this software so hopefully this is a silly question that is easily answered.I keep running into an issue where I can make a change in the editor, build the project and then look at the code step by step in debug mode, however...

0693W00000BcOAAQA3.png
RMyer.1 by Associate III
  • 2068 Views
  • 4 replies
  • 0 kudos

Freezing of stm32cubeIDE 1.5.1 on Ubuntu 18.04

Hello Dear, I have downloaded stm32cubeIDE 1.5.1 and install it. Troubles come when I launch the apps, it started and completely freezes and I could do anything before it shutdowns. Here the error messages that I get. Any suggestion? 

0693W00000BcFxrQAF.png 0693W00000BcFxhQAF.png
LBadi.1 by Associate II
  • 1464 Views
  • 2 replies
  • 1 kudos

Does STLINK allow debugging with breakpoints?

I am using a Nucleo-64 with the STM32F070RB on it with the STM32CubeIDE and I can flash my code to the memory but all I can do in debug is halting the CPU and reading out the registers. No user variables are allowed to be tracked and no breakpoints ...

MPers.1 by Associate II
  • 2194 Views
  • 5 replies
  • 0 kudos

Resolved! ULINK2 debugger

Hello,can the ULINK2 debugger works in the STM32CubeIDE?In case, how the Debug Configuration has to be set?ThanksMaurizio

LaoMa by Associate III
  • 2699 Views
  • 1 replies
  • 0 kudos

Flash corrupted, showing ? (Question mark)

I am working with STM32CubeIDE on device STM32H743I am working with the flash and sometimes the data inside them being corrupted, showing ?.What may be the reason causing some of the memory to show ?.How can i identify that without getting hardfault?...

DVars.1 by Associate II
  • 3361 Views
  • 7 replies
  • 0 kudos

STM32CubeIDE include src from other Project in the workspace

I build a project in the CubeIDE (program-project). Late i decide to make some Test for this project in another project(testing-project). Know i want when i build the testing-project, that it directly take the sourcefiles from the program-project. So...

JMüll.2 by Associate II
  • 1349 Views
  • 1 replies
  • 0 kudos

Using std::mutex with STM32H7B3I

I got an error when try to use std::mutex, std::lock and similar.There is a define _GLIBCXX_HAS_GTHREADS that prevents compiling of .Is there a way to define it from compilation or an implementation of std::mutex in RTOS?Best Regards

FMarr.2 by Associate III
  • 3243 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.