2021-06-30 1:51 AM
I build a project in the CubeIDE (program-project). Late i decide to make some Test for this project in another project(testing-project). Know i want when i build the testing-project, that it directly take the sourcefiles from the program-project. So in both project are used the same sources.
I include the headerfile from program-project in the testing-project with:
"${workspace_loc:/program-project/inc}"
so the include file are found.
but whene i try to build i get the error that the referenc to the function are undefined.
2021-06-30 2:19 AM
Okay, found a way to include the sourcfile
Settings=>C/C++ General=>Paths and Symbols=>Source Location=>Link Folder
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.