STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Nucleo project hung in system memory

Using STM32CubeIde 1.6.0.Using ST-LINK on NUCLEO-l4r5zi for debug.Create a new project selecting NUCLEO-l4r5zi board.Build with default settings - able to debug and step through main().Add printf("Entering while loop\n") just before final while(1) lo...

RHerm.3 by Associate III
  • 1251 Views
  • 2 replies
  • 0 kudos

Resolved! which is best IDE for STM32.

I am using only I2c ,USB and I2s in the STM32 MCU. May I know, Is there any other IDE that is better to replace STM32cubeIDE or it is the better choice.

AR.7 by Associate II
  • 2938 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE import from Raisonance Ride7?

Hi,We have some old projects in Ride7, but we want to stop using Ride7 to work on them. It would be nice to use STM32CubeIDE for these projects. Is there any way to import a Ride7 project, or would I have to build up the project in STM32CubeIDE from ...

andyn_ff by Associate II
  • 1794 Views
  • 2 replies
  • 0 kudos

Chinese characters?

Hello I can enter Chinese characters into the C/C++ editor of STM32CubeIDE ?And how to avoid that already written Chinese character will be interpreted in wrong way in new opened files?i.e. in windows, you can set the non standard character set for ...

LaoMa by Associate III
  • 2431 Views
  • 2 replies
  • 1 kudos

How to use STM32CubeIDE to load hex file on target?

I am using an STLINK V3 and STM32CubeIDE V 1.6.0....I would like to load a hex file instead of the debugger .elf file onto the target. I have followed the online steps and created the hex file....Can someone tell me the steps needed to point STM32Cu...

SWenn.1 by Senior III
  • 12371 Views
  • 4 replies
  • 0 kudos

STM32F746G-DISCOVERY, STM32CubeIDE, FLASH

Hello! While writing a program for writing data to FLASH, communication with DISCO is disabled. It cannot be recreated. DISCO is unusable. Can you protect yourself against it? greetingsAndrzej

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.