STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to define a specific address location to store data

Hi All, I'm using STMCubeIDE for an assembly project and I want to be able to store some variables in Flash memory at a specific address (like data tables).I tried using a command like this but it didn't work:#pragma location=0x08001000DataStart:   ....

RMyer.1 by Associate III
  • 5849 Views
  • 5 replies
  • 1 kudos

USB and USART1 Pin conflict

Hi,Iam using STM32F078VB (LQFP100 package) for my application. I want to use both USB and USART1 as UART1(asynchrounous mode) in my application. There occurs pin conflict while using USB pins and USART1 RTS/CTS pins, So I have disabled flow control (...

0693W00000CzzPHQAZ.png
maha1 by Associate
  • 1923 Views
  • 1 replies
  • 0 kudos

How to add the CMSIS WiFi drivers to a STM32CubeIDE project?

I need to add support on a STM32 MCU to a WizFi360 WiFi module and noticed it is supported by CMSIS (https://arm-software.github.io/CMSIS-Driver/General/html/index.html), is there a specific way to add these CMSIS wifi drivers to an existing STM32Cub...

FGome by Associate II
  • 2343 Views
  • 2 replies
  • 0 kudos

Why is my #ifdef not working correctly?

I have a __BOOTLOADER symbol defined for my project as shown in the attached image I want to display firmware version based on the defined symbol so I have an #ifdef statement to select the correct string. The IDE displays the source code correctly:...

0693W00000CzdxqQAB.jpg 0693W00000Czdy5QAB.jpg
gsieb.1 by Associate II
  • 9486 Views
  • 7 replies
  • 0 kudos

PDM2PCM library

Hi, I am planning to convert PDM samples received from MP34DT05TR-A to PCM samples with 24 bit resolution at 48KHz sampling frequency using PDM2PCM library in stm32f401RE MCU. As per document PDM2PCM library only gives samples with 16 bit resoluti...

KK Y.1 by Associate II
  • 917 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.