STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to compare Build Configurations

I've inherited a project that contains 10 build configurations. In the STM32CubeIde properties windows I cannot find any differences between a couple of the configurations. There are so many settings in various windows, tabs, etc. Instead of selec...

gsieb.1 by Associate II
  • 3181 Views
  • 3 replies
  • 0 kudos

Resolved! SWV not working with STM32L475

SWV trace and printf not works with my Discovery board STM32L475​VGT6 MCU. I am using using micro USB for connecting board with PC. How can I trace using SWV

SSIVA.1 by Associate
  • 1438 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H723 SVD file incomplete

Definition of I2C5 is missing from the STM32H723.svd file found in STM32CubeIDE 1.6.1 installation directory.Is this a mistake or by design? Because of this I can't access I2C5 control registers in the debugger.

HWidj.2 by Associate III
  • 2568 Views
  • 2 replies
  • 0 kudos

Missing Flash-Programming progress bar in CubeIDE

Hello.I'm using CubeIDE V1.7.0 in combination with an ST-Link V3.Is there a possbility to view a progress bar that shows the progress of the flash-programming (compare, erase, program) sequence?Segger J-Link includes this progress bar overlay in the ...

0693W00000D0IhFQAV.png 0693W00000D0IhPQAV.png
PKrau.1 by Associate
  • 1345 Views
  • 1 replies
  • 0 kudos

Inconsistent vector table on Nucleo with STM32L4R5

I have a project, created with STMCubeIDE 1.6.1, for a Nucleo STM32L4R5 board. I experience issues with the vector table not being always the correct one, depending on some influence I'm not quite sure about. Let me explain.The project has a few peri...

Kemaguco by Associate II
  • 3815 Views
  • 6 replies
  • 0 kudos

STM32F446RE - Disable PA0 (Reset Button) to run the code

Hi,I'm currently using the STM32F446RE with the STM32CubeIDE. My problem at this moment is, after flashing the code it only runs when I debug through CubeIDE, but if I connect the USB it is necessary that the B2 (PA0) is pressed for the code to start...

JOlse.1 by Associate
  • 1851 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.