STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Getting "Error: Target not available" in Value column in live expressions in StmcubeIDE in debug mode when i press Resume(F8)

I created a simple GPIO program with the code generated from StmCubeMX. When i build the program there are no errors and warnings, but when i connect my Nucleo-F411RE and try to debug it, i get this message in Expressions.The program is supposed to m...

0693W00000DnuFCQAZ.png 0693W00000DnuEsQAJ.png

Resolved! How to correctly uninstall and reinstall the stm32cubeide?

Hi,(1) Is it ok to install the IDE as my user and not via sudo? It seemed to be ok until I had some later issues which I wont go into here just yet as almost certainly "user error".(2) I installed the ide (as user), and because it was saying it could...

rileyrg by Associate II
  • 15103 Views
  • 2 replies
  • 2 kudos

I keep on running into -> void HardFault_Handler(void); When my HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *) pwmData, index); Is called

Hi. I seem to get HardFault_Handler error when I start my HAL_TIM_PWM_start_DMA function.I am not sure if it just gets stuck in an infinite loop in the while() called right after it.This looks like allot of code but really its just 5 of my functions ...

CMcC.1 by Associate II
  • 2089 Views
  • 3 replies
  • 0 kudos

Resolved! How to reasonably use git source control

I'm trying to create process for development with CubeMX/CubeIDE projects.I'm seeing pathing issues that show up when my project is moved. Which also means when it's cloned to another computer.Simple steps I've done to reproduce this:Created a new pr...

0693W00000Dmq5uQAB.png 0693W00000Dmq6JQAR.png

Resolved! Is there a panel to shown warnings in STM32CubeIDE?

HelloI'm using 'STM32CubeIDE 1.7.0'.I've copied a project using: The new project failed the first time I built it as the User Code in main.c had not been copied over. Once I added this missing code the project compiled and ran correctly on the Nucleo...

0693W00000DneRqQAJ.jpg 0693W00000DneRvQAJ.jpg
ron_w by Associate III
  • 3550 Views
  • 2 replies
  • 0 kudos

Must reconnect Nucleo to USB in order to run code

I have a simple cubemx generated project where i simply toggle led and printf to my external console. After programming the program isnt running. i must reconnect the st-link usb interface and then the program will run normally. Simply pressing re...

Rshaw.1 by Associate II
  • 2611 Views
  • 4 replies
  • 0 kudos

Resolved! Intermittent Break at address "0x1fff51f4" with no debug...

Hardware:MCU: STM32L4R9ZGJ6 (Custom board)OSPI mapped to address 0x90000000ST-Link V2PH3-BOOT0 pin pulled to ground with 10k Ohm resistor.Software:IDE: STM32CubeIDE 1.6.0 (Build: 9614_20210223_1703 (UTC)SDK: STM32Cube_FW_L4_V1.14.0TouchGFX assets are...

DerekR by Senior
  • 22793 Views
  • 42 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.