2021-09-20 9:55 PM
Hi,
(1) Is it ok to install the IDE as my user and not via sudo? It seemed to be ok until I had some later issues which I wont go into here just yet as almost certainly "user error".
(2) I installed the ide (as user), and because it was saying it couldn't download firmware, I decided to remove it (rm) and reinstall. It says "nothing to install" despite the --target directory AND the previous workspace being non-existent.
So from (2) how is it determining there is "nothing to install" when I have nothing installed?
I'm very new to this IDE so please be patient ;)
Solved! Go to Solution.
2021-09-20 11:16 PM
Hi @rileyrg,
Steps are described in this topic: https://community.st.com/s/question/0D53W00000IreG7SAJ/how-do-i-properly-uninstall-a-previous-cubeide-version-in-linux
Hope this helps.
2021-09-20 11:16 PM
Hi @rileyrg,
Steps are described in this topic: https://community.st.com/s/question/0D53W00000IreG7SAJ/how-do-i-properly-uninstall-a-previous-cubeide-version-in-linux
Hope this helps.
2021-09-20 11:52 PM
Oh, was an early start. Cant believe I didnt find that. Thanks.
I added a couple of facility scripts that some may find helpful. I use sway/wayland so needed to do the x11/reparenting thing.
https://github.com/rileyrg/linux-init/blob/master/directories/bin/stm32cubeide-uninstall
https://github.com/rileyrg/linux-init/blob/master/directories/bin/stm32cubeide
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.