STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to write a bin file with a start address in stm32cubeIDE. Also, how to debug App in a project with separate Boot and App?

I am using an STM32 system with separate bootloader and application parts implemented. This time I want to modify and debug the application part, but I don't know how to achieve that in STM32CubeIDE.I would appreciate your advice.​*The path of gdb an...

MYMM by Associate
  • 6020 Views
  • 4 replies
  • 0 kudos

Help, looks like I broke Cube IDE (initialization problems)

Today, I opened a new project, exactly the same way I did all the previous ones. I selected the STM23F413ZH Nucleo-144. ​Unfortunately, I didn't get a "Do you want to initialize all peripherals in their default modes?" this time. When the IOC file fi...

MPave.2 by Associate
  • 6056 Views
  • 3 replies
  • 0 kudos

Hi, Has any one tried importing the 'voltage mode buck example project' as available for download here: www.biricha.com/ST-Discovery-Kit into the STMCube IDE?

The reason I ask is, the application note 'an5496-buck-voltage-mode-with-the-bg474edpow1-discovery-kit-stmicroelectronics' says the Buck_VoltageMode_SW.ioc is setup to be used with IAR workbench. However the same application note also mentions 'STM C...

vchilapu by Associate II
  • 869 Views
  • 0 replies
  • 0 kudos

How to use old HAL library in CubeIDE

Hi, I have a problem using stm32f722 uC with HAL 1.16.0 and 1.16.1I write a simple UART send project and test it with an oscilloscope (becouse it doesn't work with the target device) and discover that HAL_UART_Transmit is sending correct bytes while ...

Lgarb.1 by Associate II
  • 4941 Views
  • 9 replies
  • 0 kudos

Resolved! How does one observe peripheral registers with CubeIDE?

Remedial register view help needed.I need to see DMA and UART registers, not having much luck.ron239955_stm1 referred to the i/o registers window, how is this done?From Debug Perspective, Registers View, I see only General Registers.I notice that the...

Sking.21 by Associate III
  • 5805 Views
  • 3 replies
  • 0 kudos

Break-point issues on STM32G030F6P6

Hi,When I try to upload to my STM32G030F6P6 I get the following error and sometimes I get the "Command Aborted" message attached in the picture.I tried resetting my workspace too. But still I get this error. Erasing memory corresponding to segment 0:...

0693W00000GY7yjQAD.jpg
Sahiru by Associate II
  • 1776 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.