STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE 1.8.0 and C++17 support

Hello.CubeIDE 1.8.0 now includes STM32 toolchain based on GCC 10.3.1 which supports C++20, but the IDE still can't correctly parse C++17 syntax, like Class Template Argument Deduction guides. I tried to force '-std=c++17' option to Language Settings ...

Files left over from code geneation in StmCubIde

Hi everyone, Any of you experienced this strange behavour posted yesterday (see below)? It seems to happen to just one of my projects, and not all of the source files are affected (but still a substantial number of files). Any thoughts and experien...

Per4 by Associate II
  • 1083 Views
  • 0 replies
  • 0 kudos

Resolved! Stm33cube ide with iar or Keil compiler

Recently I read that iar or Keil are better compiler than GCC. However I can not say the same for the IDE. So I don't want use another ide and I just want to use another compiler. Is that possible?​​

JCuna.1 by Senior
  • 1785 Views
  • 1 replies
  • 1 kudos

Anyone had any luck using a DM9051 via SPI?

I have a need to have incoming serial data go out via UDP and thought of using a F030F4 as it doesn't need to do much just in to out.I ordered some boards from Amazon (yes) and they look small and are inexpensive, all the offered code is set for a Ke...

SScot.3 by Associate II
  • 975 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CubeIDE stealing focus

Is there a way to disable STMCube IDE from constantly stealing focus? I'd rather get to it when I'm done with another window than be interrupted Clippy style ;)

JMath.2 by Associate II
  • 2989 Views
  • 5 replies
  • 0 kudos

Resolved! HAL for I2C is horribly broken

Hi STM Community,I would like an answer from STM about the status of I2C in the HAL drivers.Basically, they are broken, and still broken in STM32CubeIDE-1.7.0.Of the many issues, there is still an open one here: https://github.com/STMicroelectronics/...

etheory by Senior II
  • 9237 Views
  • 9 replies
  • 2 kudos

Resolved! Hi The goal is to convert the Sigfox_Button example in STSW-S2LP-SFX-DK from Keil IDE to STM32CubeIDE.

I adjust the code and now I don't have compiler errors but I have 3 link errors. The 3 library that I added in the link section are not found. I remove the extensionwhen add them in the list and set the files correct path.The attachments show my sett...

trx2001 by Associate II
  • 3700 Views
  • 3 replies
  • 0 kudos

Resolved! Will there be any toolchain updates?

Hi All,today I have installed new STM32CubeIDE 1.8.0. Despite the current toolchain 9-2020-q2 is very old the new IDE does not update it. Will there be any GNU Tools for STM32 updates, or I should now use GNU Tools for ARM?Regards,Dmitry

DmRozhd by Associate III
  • 5353 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.