STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Potential bug of STM32CubeIDE Version 1.9.0

Hi everyone, I don't know if this is the correct section, if not, I'm sorry, maybe you can move it to the correct section. I wanted to report a potential bug of STM32CubeIDE Version: 1.9.0, Build: 12015_20220302_0855 (UTC). The card I am using is the...

PGius.1 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

Resolved! An issue with IDE 1.9.0 with dual-core STM32H7

The board I'm using is NUCLEO-H755ZI-Q and it has two cores, a Cortex-M4 and a Cortex-M7.After I update STM32CubeIDE to Version: 1.9.0, I can't download programs to the core Cortex-M4. I've already updated ST-Link to the latest version.It says:STMicr...

TKuo.1 by Associate III
  • 1341 Views
  • 1 replies
  • 0 kudos

[BUG REPORT] ADC DMA error on new HAL for STMCubeIDE 1.1.0

Tested on STM32F334R8 nucleo board. Attempting to stop ADC in regular dual simultaneous mode doesn't work in latest HAL, though does work for prior version of the IDE 1.0.2. Do something like this to reproduce:void HAL_ADC_ConvCpltCallback(ADC_Handle...

escher by Associate II
  • 1207 Views
  • 1 replies
  • 0 kudos

Resolved! Issue using pointers

Hello,can someone help to identify where is the issue using pointers? The code example is below.On line 36: workMode->current = workMode->intend;It's not overwriting/changing the value.If I change it to like this:*workMode->current = *workMode->inten...

RZub by Associate II
  • 3614 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.