STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Search for the best way to change controller in cube IDE.

Hi,What is the most efficient way to change controllers on a custom board?I have changed the STM32G473RE to an STM32G473RC, the project is build and compiled with cube IDE (so i have an ioc file too). Is there an easy way to change the controller in ...

sde c.1 by Senior II
  • 3991 Views
  • 5 replies
  • 1 kudos

Resolved! Is there an option to build code for different MCUs of same architecture with the one *.ioc file in STM32CubeIDE?

As part of maintaining one repository for the application SW, planning to make HAL separation and build configuration switch to be able to work with one STM32CubeIDE, ioc file.Controller change expected from the same Architecture. listed as below Cur...

Seenu by Associate II
  • 5454 Views
  • 6 replies
  • 0 kudos

Resolved! Genereta report with STMCubeIDE problem

There is option generate report in STMCubeMX but I didnt find on STMCubeIDE. Where is the this option. ("generate report" )  With the Generate report, you export the configuration settings of the project we created in STMCubeIDE.

0693W00000KdjKxQAJ.png

Resolved! Hello, I have updated my STM32CubeIDE from V1.7.0 to V1.9.0. After that my project fails to link with > 40 000 "multiple definition of" errors. Before the project was compiling for years without such problems.

I chaecked the following:There are no variable definitions in my headers. I use #ifndef/#define/#endif in all headers. After 2 days of trying I don't know what to do anymore. What might have changed in V1.9.0?

JBurg.5 by Associate II
  • 3585 Views
  • 6 replies
  • 0 kudos

Failed to start GDB server

hi guyscould you help me to fix this problem ?i can programming my program with STM32 ST-LINK Utility and its worked but when i use Run OR Debug in stm32cubeide it does problem my board and my programmer is in the attechments

Issue with IDE 1.9.0 and 1.10.0 with STMH7 RTOS + LWIP

I have a project using both RTOS and LWIP. I updated my IDE today and the project will not compile I get the following error below that errno is declare multiple times. errno is only declared once in the project. Even if I create a project with RTOS ...

DCorn by Associate III
  • 2298 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.