2020-03-31 1:45 PM
hi guys
could you help me to fix this problem ?
i can programming my program with STM32 ST-LINK Utility and its worked but when i use Run OR Debug in stm32cubeide it does problem
my board and my programmer is in the attechments
2020-03-31 4:58 PM
Have you imported the project from other OS (Windows vs Linux) and use existing debug configuration?
If so, delete the debug configuration and create new one.
-- pa
2020-04-01 2:28 AM
thanks for response,
no i didnt
i have same problem with cubemx when i generate code for keil it has problem i search about that and i noticed that we should install jdk 8 but i have android studio with jkd version 13 and i cannt delete it possible this problems beacuse of jdk version???
2020-04-01 3:49 PM
Java versions is a different problem. The debugger engine (iether OpenOCD or gdb server) do not use Java.
If you have Keil, the debugger is different there and may work much better.
-- pa
2020-04-02 1:48 AM
I tired of stm32cubeide it does error gdb server
I can program with keil and its work on my board but it has problem too, when i want to program or debug it take error "Not a genuine ST Device! Abort connection"
Also I upgrade firmware st link
2020-04-13 4:39 AM
I have this error too(( IDE #1.3.0 for macOS
2020-04-15 2:32 AM
Добрый день, Павел. С �?той ошибкой иногда �?талкиваю�?ь - непред�?казуемо - в проце�?�?е работы. Пока вывод - не оригинальные Сви�?тки �? �?лиек�?пре�?�?, к�?тати за 2 недели внезапно умерли 2 штуки((( - они давали большую ча�?ть ошибок . По�?тавил оригинальный st-link2 == 2 дн�? полет нормальный. Один умерший Сви�?ток �?ам переделал дл�? отладки (вывел �? него на те�?тируемую плату линии SWO + RST, необходимо�?ть RST в данном варианте отладки SWV так и не пон�?л - работает и �?ни и без, вкл. программный ре�?ет)
2020-04-15 11:34 AM
can you speak english?i cannt understand what did you say
2020-04-15 12:46 PM
You can try Google Translate, I am using too - I dont speak English - all forumes translate Google ))
2020-04-15 12:48 PM
�?нглий�?ки�? �?зык не един�?твенный в мире)) Гугл предо�?тавил нам прекра�?�?ную возможно�?ть на уровне Э�?перанто))
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.