STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Display problem in the IDE with #if and #ifdef

Hello, I am working on a project with a dual core processor (H7) and I have some display problems in my IDE (STM32CubeIDE v1.9.0). For example, I added the LWIP part to my board with #define LWIP_IPV4 1 and #define LWIP_DHCP 1.When I am in debug mode...

MA4 by Senior
  • 3638 Views
  • 6 replies
  • 0 kudos

STM32L476 comparator constantly generates an interrupt

Hi. I configured comparator with neccessary settings using CubeIDE and LL library and got next generated piece of code: COMP_InitStruct.PowerMode = LL_COMP_POWERMODE_HIGHSPEED; COMP_InitStruct.InputPlus = LL_COMP_INPUT_PLUS_IO1; COMP_InitStruct....

ARa.2 by Associate II
  • 2334 Views
  • 2 replies
  • 0 kudos

Resolved! Failed to enable Live Expressions. Connection failed

Can't enter into the debug mode on the development branch, but when I switch to master branch I can normally use the debugger. Difference between master and dev branch is minimal, and projects settings and debugging configuration is the same. I've tr...

0693W00000UoXLHQA3.png 0693W00000UoXK5QAN.png
DCind.1 by Associate
  • 6604 Views
  • 2 replies
  • 0 kudos

Want a Buffer to Buffer compression (.zip) library

Hi all, I am using STM32 F411 Discovery board and am facing an issue with compression, i tried different compression libraries (zlib, mzip etc) all are using File system, unfortunately the F411 Discovery does not supporting Local File system, my conc...

How to build headless inside a docker container

I've installed STM32CubeIDE inside a docker ubuntu image.If I start my docker-image and mount the folder with my source code (base directory is called 'primary' and hostmachine is a MacBook), and run this command:/opt/st/stm32cubeide_1.10.1/stm32cub...

JAnde.15 by Associate
  • 1520 Views
  • 1 replies
  • 0 kudos

Ethernet not working

Hello community, I'm usingSoftware:-STM32CubeIDE v1.10.1--STM32Cube FW_F4 V1.27.1Hardware:-STM32F4Discovery-PHY DP83848-RJ45I want to implement the Ethernet peripheral in the STM32F407 mcu with RMI mode without RTOS (via polling mode), and I used stm...

QSDFG.1 by Associate
  • 1189 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.