2022-10-21 12:57 AM
Hello, I am working on a project with a dual core processor (H7) and I have some display problems in my IDE (STM32CubeIDE v1.9.0). For example, I added the LWIP part to my board with #define LWIP_IPV4 1 and #define LWIP_DHCP 1.
When I am in debug mode, I can see that I pass in the code present in dhcp.c (starting with #if LWIP_IPV4 && LWIP_DHCP) but the code is totally greyed out as if LWIP_IPV4 and LWIP_DHCP were 0.
This is an example, I can observe this phenomenon elsewhere in my project.
Does anyone have a solution?
2022-10-21 1:51 AM
(in C) really : >> #if LWIP_IPV4 && LWIP_DHCP << ? warning ?
#ifdef LWIP_IPV4
2022-10-21 2:27 AM
OK but it's not my code but the LWIP middleware files.
plus I don't want to modify the middleware or driver files because I can't update them if I do
2022-10-21 1:51 PM
2022-10-22 5:38 AM
ok, ... so maybe you need to have a C++ project, in c++ "#if ..." should be doing, what you want .
+ in IDE : right click on your project -> option: convert to c++ (try, but first backup your project ! )
2022-10-26 12:01 AM
I close my project and open it and the problem has disappeared in many files
2022-10-26 12:04 AM
Yes, it's help but I don't want to duplicate files, I know it's can works without, maybe it's a loading problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.