STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1702 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STMCubeIDE not opening ioc in MX mode

My STMCubeIDE is not opening the ioc files or creating STM32 projects, it is acting like the ioc files are text files, not using the STMCubeMX mode to open them. I'd already tried reinstalling the STMCubeIDE a few times, in the C folder and in other ...

New STM32CubeIDE Version 2.0.0

Hi I have installed the updated version V2.0.0 and tried to configure the MCU like before using GUI , but it is not supported then how to get GUI like CubeMX version to configure microcontroller, please help  

Thsl by Associate II
  • 1072 Views
  • 3 replies
  • 1 kudos

Resolved! GitHub Copilot seems broken (Cube IDE 1.19)

Running ST Cube IDE 1.19 on Windows 11, co-pilot autocompletions seem to be causing an issue. I see the suggestion, then a dialog pops up saying the following:An internal error occurred during: "Generating completion...".Invalid thread accessI look a...

NickO by Associate III
  • 1948 Views
  • 15 replies
  • 2 kudos

Resolved! Missing value in the STM32CubeIDE SFRs window

While testing the X-CUBE-EEPROM library in STM32CubeIDE (v1.18.1), I observed the FLASH->CR register in the SFRs window. I noticed that the display for BKER (bank erase select bit) is missing in the FLASH_CR register. Please try to correct this in th...

BPrem.1 by Associate III
  • 1157 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE 2.0.0 released

We are pleased to announce that STM32CubeIDE 2.0.0 release is available. STM32CubeIDE is now independent from STM32CubeMX. With this release, device configuration, previously handled within STM32CubeIDE via STM32CubeMX, is now exclusively available t...

Aimen1 by ST Employee
  • 15551 Views
  • 0 replies
  • 6 kudos

Garbled Font in the title of the IDE window

As shown in the figure, the title of the window bar seems to have become garbled, even though its content was originally in English. I thought it was due to the software defaulting to a font that only supports Western characters, but changing all the...

Altboy23 by Associate
  • 565 Views
  • 1 replies
  • 0 kudos

STM32H755 dual core SWO printf

Hi,I would like to get printf() debug messages from both M7 and M4 core using SWO pin. It seems to work as expected on M7 core, but I cannot get it work on M4. Ideally, I would like to have messages from both cores in parallel, but it would be great ...

mosamasa by Associate II
  • 443 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.