STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Getting error "Could not verify ST device" in CM4 core when debugging STM32H745I-DISCO board using SWD mode in Segger J-link.

I am working on following platform:Hardware - STM32H745I-DISCO board.IDE - STM32CubeIDE v1.10.1.STM32CubeMX v6.6.1-RC2.Embedded MCU package for STM32H7 v1.10.0.I am using SWD mode in Segger J-link for debugging. I am getting error "Could not verify S...

Akast.2 by Associate II
  • 5577 Views
  • 5 replies
  • 0 kudos

Trying to print float value using stdarg.h file in CubeIDE

I'm using an STM32F4 mcu to receive data from a sensor. Now i want to print that same data which is in float. I've tried using functions like snprintf/sprintf but they give some error about linker flag. Now i've tried to add -u_print_f in the linker ...

IHiro.1 by Associate
  • 1428 Views
  • 1 replies
  • 0 kudos

Hey :) I am trying to flash my program onto my stm ucontroller but I get a libusb error message. Can you help me please?

I'm using STM32Ide. I installed pypy libusb1 and python3-libusb1 in the software manager of linux mint (I am using linux mint 19.2). I thought I need some libusb to solve the problem but I couldn't solve it. I couldn't find a guide. I want to flash m...

0693W000000XFPqQAO.png 0693W000000XFPlQAO.jpg 0693W000000XFPbQAO.jpg
Ykost.1 by Associate
  • 5705 Views
  • 8 replies
  • 0 kudos

undefined reference to `__fabs'

I want to use the intrinsic floating point absolute value function `__fabs` as noted in the compiler specific features in the armcc documentation.When I build my project using the following settings on STM32CubeIDE: I get an error saying undefined re...

0693W00000Y8SHHQA3.png
DLian.3 by Associate II
  • 3789 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.