STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! nucleo-L476 / RealTerm / printf not working??

Hello All...I am trying to send data to realterm using printf....I used cubemx to set up baud rate, etc. and have called MX_USART2_UART_Init. RealTerm is pointing to the correct serial port with the correct baud rate....A breakpoint validates the da...

SWenn.1 by Senior III
  • 2725 Views
  • 3 replies
  • 0 kudos

Resolved! strncpy_s in STM32: undefined reference to `strncpy_s'

Hi. I have the following code:messageprocesser.h#ifndef INC_MESSAGEPROCESSER_H_ #define INC_MESSAGEPROCESSER_H_   #ifdef __cplusplus extern "C" { #endif   #include "main.h" #include "usbd_cdc.h" #include <stdint.h> #include <string.h> #include <stdio...

0693W00000YA3UPQA1.png
OIp.1 by Associate III
  • 5224 Views
  • 4 replies
  • 0 kudos

Ethernet with Nucleo-144 STM32F746GZ did not work with STM32CubeIDE 1.10.1 and STM32F7 library 1.70.1. The CubeMX is 6.6.1.2.

The Nucleo-144 F746GZ board worked fine with legacy Ethernet FW from System Workspace (as well as demo FW from System Workspace). I have added PG12 for Phy Reset however I am unable to get ethernet up via a twisted ethernet connection to the laptop. ...

Riscy by Senior
  • 6290 Views
  • 16 replies
  • 1 kudos

Resolved! How to add .o file in STM32 cube IDE

Hello all,I have referred the STM32cubeIDE user manual and found the procedure to add the .o file to the project.I want to call a function from the added .o file.But I get the following error.../Core/Src/main.c:130:3: warning: implicit declaration of...

Aarra.1 by Senior
  • 2898 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 IDE type and list down function/variable suggestion list

I saw some tutorials with STM32 IDE 1.11.0, > When typing for the variable or function name, it makes a list and selected if found.and I don't see it doing that; where is the configuration in preference top enable it or was is it from the plugin fea...

Riscy by Senior
  • 4379 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.