STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

No rule to make target `clean' ?

Hello,I use STM32CubeIDE v 1.4.2 It appeared today during the build my project:make clean make: *** No rule to make target `clean'. Stop."make clean" terminated with exit code 2. Build might be incomplete.11:48:08 Build Failed. 1 errors, 0 warnings....

Peko by Associate III
  • 11361 Views
  • 7 replies
  • 1 kudos

Resolved! CMake 3.20 or higher is required

HI I try to import my Stm32cubeIde project into VSCodeI have install STM32CubeCLTthe configuration failed with this error [variant] Loaded new set of variants[kit] Successfully loaded 5 kits from C:\Users\XXXXXX\AppData\Local\CMakeTools\cmake-tools-k...

LHOUE by ST Employee
  • 4573 Views
  • 4 replies
  • 0 kudos

Host process of CDC (Virtual Port Com) does not work.

I am using STM32G0B1KC to make a CDC class USB Host.I selected in STM32CubeIDE, Mode=Host_Only (FS) in Connectivity - USB_DRD_FS and Communication Host Class (Virtual Port Com) in Middleware - USB_HOST.Before creating the user program, I checked the ...

JJ4IQV by Associate
  • 4317 Views
  • 7 replies
  • 0 kudos

Writing to flash bricks stm32G030 and stm32G031

If I create a program using stmcubeIDE and ADD the code below it bricks the processor . I gather in some way I am overwritting the bootloader that controls stlink and get the errorTarget no device foundError in initializing ST-LINK device.Reason: No ...

PGood.1 by Associate II
  • 2907 Views
  • 3 replies
  • 0 kudos

Debugging with GDB server localhost doesn't work

STM32CubeIDE for MAC Version: 1.12.0Just installed the tools and connected an STM32 Nucleo 144 for the first time.After connecting it, a ST-Link upgrade window popped up about updating the firmware of the board which I did. Got the Upgrade successful...

0693W00000bhQI5QAM.png
MMain.1 by Associate II
  • 3613 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.