STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE suddently stop to Debug and Run

Hi there, I'm facing a problem with Cube IDE (ver. 1.13.0). Completely out of nowhere, it stopped letting me debug or run the code. When I click the buttons, I can see in the bottom right corner that it tries to launch the debugger, but it stops at L...

SScar.2 by Senior
  • 2758 Views
  • 2 replies
  • 1 kudos

STM32G031 SPI read problems

i am using the STM32G031 and the SPI1 port. i have used the SPI port many times on various STM32F devices. I have found some of the STM32G devices have odd behavior. Today i have a strange problem i am running 16 bit SPI1 and when i observe the wavef...

Resolved! STM32H723ZG USB CDC ADC DMA

I am using STM32H723ZG nucleo board. When I enable HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_buf, ADC_BUF_LEN); USB Virtual port doesn't show up and when I disable it, it shows up. Can anyone explain what could be the issue?I was able to print "Hello"...

AKhot1_0-1693307526832.png AKhot1_1-1693307704147.png AKhot1_3-1693307747447.png
AKhot.1 by Senior
  • 3204 Views
  • 4 replies
  • 0 kudos

Help using SWD and NRST as GPIO safely - STM32G031

Hi, so I've chosen to use STM32G031J6M6 8-pin version for an audio level meter project to get me started. I'm using pin 1 as the adc input, 2 and 3 are 3v3 and gnd, obviously. I was hoping to use the remaining 5 pins as GPIO outputs attached to LEDs ...

NGD by Associate II
  • 9920 Views
  • 11 replies
  • 1 kudos

STM32CubeIDE Mass Erase rather than Sector Erase

I have a STM32H723 on a custom board that I'm having a lot of trouble programming. Every time I try to flash it, the erasing of flash sectors fails. I can, however, perform a full chip erase. All the option bytes are configured as they should be, but...

Iris-DM by Associate III
  • 2504 Views
  • 1 replies
  • 0 kudos

Hard Fault handler FFT

After the arm_fft function, I am running into a hard fault handler when running in debug mode. I am not getting why is it happening. Please help with this. Is it because of some wrong memory allocation? 

AKhot1_0-1693225742548.png
AKhot.1 by Senior
  • 3626 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.