STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F303ZE ADC data display on PC

I want to use my STM32F303ZE board as a high speed data taker from outside ADC pins, and display these (large amount of) data on my computer. I am now using an SD card to store the data on my board. How can I display the taken data from the ADC pins?

elif79 by Associate
  • 1341 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CUBEIDE Interrupt Vector Table does not correctly

Hi I am trying to implement my own drivers in order to learn C++ for embedded. I am working with a STM32F407G (discovery board). I was trying to implement a Handler for SysTick but for some reason when I look into the vector table in memory, SysTick ...

erenimo by Associate
  • 2175 Views
  • 2 replies
  • 1 kudos

Resolved! Headless build fail on linux STM32CubeIDE v1.13.1

OS: Ubuntu 20.04.6 LTSSTM32CubeIDE version 1.13.0 or 1.13.1My project builds fine in the IDE and with headless builds on version 1.12.1. With version 1.13.X builds within the IDE work fine, but attempting a headless build from command line fails near...

Marshall by Associate
  • 3980 Views
  • 3 replies
  • 3 kudos

Not receiving data from STM 32 Nucleo

In this code, when I use the temp command, I always get output as "No response received." That means my python CLI is not receiving any data from the STM 32 board. But when I run the same command on the screen terminal on my mac, I get the data. What...

Xx11 by Associate
  • 1168 Views
  • 0 replies
  • 0 kudos

Feasibility of a project on nucleo stm32h7 platform

The objective is to visualize the response of a device to a series of pulses of different durations.The number of pulses, their duration and their frequency are given as an indication and can be adapted.I want to acquire several identical pulses to i...

Alban48 by Associate II
  • 4584 Views
  • 6 replies
  • 0 kudos

STM32F4 Discovery ST-LINK error

I was just uploading the code without having any issue and after the new update of Cube IDE it just does not recognise the ST-LINK of the Discovery board (STM32F469). I attach the images. I tried to reset the board but can do it via ST-LINK Utility. ...

error_1.PNG error_2.PNG ERROR_3.PNG
Enekkk by Associate II
  • 2703 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.