STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

start stm32

I wrote a program with buttons and LEDs.I wanted to continue with other peripheral devices. But unfortunately I had to reinstallWindows. And the problems started: I can neither open the previous project nor make a new one. STM32 Cube needs to be upda...

STM32WB LPSLEEP issue

Hello, I'm trying to implement Low power sleep on STM32WB. The sequence is as per LPSLEEP example:HAL_PWREx_EnableFlashPowerDown(PWR_FLASHPD_LPSLEEP); SystemClock_Decrease(); //MSI 2MHZ HAL_SuspendTick(); HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_...

MHast.1 by Associate II
  • 1681 Views
  • 1 replies
  • 0 kudos

TM32CubeIDE 1.13.1 and Nucleo-F429ZI - Linker Error

Hello,when I create a new project with Ide 1.13.1 and Nucleo-F429ZI and enable ETH,  LWIP and HTTPD then I get following linker errors. Seems some module are not compiled automatically. What could be the reason? How to solve?C:/ST/STM32CubeIDE_1.5.0/...

jens3 by Associate
  • 2146 Views
  • 2 replies
  • 0 kudos

Debugger wont launch

I've been using the STM32CubeIDE on a Ubuntu system to develop code for our STM32 based device. Up until today everything was working just fine. But today I made some changes to my code, and when I went to launch the debugger to try it out, I get n...

DTovey by Associate II
  • 10198 Views
  • 12 replies
  • 12 kudos

STM32CubeIde COMPILER

Dear Sir,A project written for STM32U585 reaches the size 900 k bytes.Trying to lower the size , I am tryin to use properties.MCU GCC C compiler -> OptimizationTrying to set Optimization level to optimize most  to -Q3 the property of Optimization lev...

CUBE IDE C code sharing

Good morning,I apologize if this question is a bit dumb, I'm still learning embedded programming.I'd like to know if its possible to share code between projects in STM CUBE IDE.The idea is to have like a "folder" with one (or many) .h and .c files. T...

BRapo.1 by Associate II
  • 2579 Views
  • 2 replies
  • 1 kudos

Middlewares deletion bug in CubeIDE 1.13.1

When reconfiguring a project using emDos and StemWin, the StemWin selection shows up under Middlewares/st, etc.When disabling emDos in the ioc file, the section for emDos is deleted, but so is the StemWin. Removing the OS also removes the entire Midd...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.