STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Project separation

I have a project for a STM32H7. The idea is to split the project into two separate projects. This is a functional separation. Can anyone help me what elementary steps are necessary to make these projects as follows:One project should land directly in...

DaBa by Associate
  • 1160 Views
  • 1 replies
  • 0 kudos

Build error log

I have recieved a project from a third party who was working on our source code. When I build, I get these errors. I am new to STM/Eclipse, so I am sort of lost on how to remedy the situation. Thanks!

MAlan.1 by Associate III
  • 1899 Views
  • 2 replies
  • 0 kudos

What is the point of this UI element?

When the project configurator will forever just generate a main.c and then never compile because 'class' type is not defined...Seriously STE... take a hint from this and below: Your IDE is bad and you should feel bad.  You have a UX, documentation, a...

capnhyaku_0-1697198402198.png

SWV ITM Data Console is empty

This problem is common, but I've reviewed my setup and everything appears to be correct, yet it still doesn't work.My programmer is an STLINK-V3PWR, connected via a 6 pin Tag-Connect (TVCC, SWDIO, NRST, SWCLK, GND, SWO) to an STM32F411CEU6.In the STM...

NateS by Associate III
  • 13479 Views
  • 14 replies
  • 1 kudos

STM32CubeIDE 1.13.2 released

STM32CubeIDE 1.13.2 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.2 that is available for download. Main issues fixed in this patch: Ticket 160463 - [STM32CubeIDE 1.13.0]Build error after calling printf.Ticke...

Resolved! DSP Installing

I've followed this tutorial to install the DSP libraries on STM32F407 discovery.Should I keep all the files in the folders in the attached picture? Or only one per folder? (i.e. according to the uController I choose which one to keep)I think I have t...

screen.png
luke514 by Senior
  • 4094 Views
  • 5 replies
  • 1 kudos

Audio file Input for DSP on STM32f4

Hello Everyone,I am working on a project involving digital signal processing (DSP) using the STM32f401 microcontroller. My goal is to integrate external audio, specifically audio recorded in '.wav' format, into my program. I've successfully incorpora...

tomstom_ by Associate
  • 1753 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.