STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Fail to execute MI command -- error message from debugger back end -- error erasing flash with vFlashErase packet

Hi everyoneI start using CubeIde v1.3.1 with a Nucleo board recently , the first project --toogle LEDIt was everything OK,was able to download ,debug and run the program into the Nucleo untilI think I did an update of the ST-Link; and since then I...

Problems with the GCC from STM32CubeIDE version 1.13.2

So.... On October 31, more than 3 month after, the last version 1.13.2 as not been updated and the problem is still present. Seriously ST, this is not professional at all! Could you test the version you are releasing!! And provide fast correction whe...

ANauz.1 by Senior II
  • 3255 Views
  • 3 replies
  • 2 kudos

Resolved! Stm32wle5jci6

I have been working in Stm32wle5jci6,im trying to integrate My I2C code with lorawan code package downloaded from github. I had tested with Macros in that case the data was pushed in Chripstack, but whenever i try to connect the sensor i am unable to...

Nani96 by Associate II
  • 2172 Views
  • 2 replies
  • 0 kudos

Failed to start GDB server today

I have a variety of projects I've been working on over the last year using a STM32Nucleo H7A3 board.. I use both the VisualGDB IDE and STM32CubeIDE. I wanted to build a FatFs project from scratch using STM32CubeIDE yesterday and got it working surpri...

_legacyfs_online_stmicro_images_0693W00000bk9buQAA.png
magene by Senior II
  • 3346 Views
  • 3 replies
  • 0 kudos

Resolved! how to switch to other task's context

I am using STM32CubeIDE to develop a product with STM32H7 chip. I enabled freeRTOS in our software system. When I debug code, I can see freeRTOS tasks in "FreeRTOS Task list window" and I am in current task context. How can I switch to other task's c...

HarryXia by Associate II
  • 2796 Views
  • 3 replies
  • 0 kudos

Pwm pin Continuous high

I am working on STM32F103 and made a pwm with TIM1 channel 1 and 2 with channel 1 non inverted and channel 2 inverted, when i am disabling the pwm using HAL the inverted channel goes to continuous high state. any kind of help will be appreciable and ...

RChou.1 by Associate III
  • 3515 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.