2023-08-16 10:51 PM
I have been working in Stm32wle5jci6,im trying to integrate My I2C code with lorawan code package downloaded from github. I had tested with Macros in that case the data was pushed in Chripstack, but whenever i try to connect the sensor i am unable to read the sensor data. Note : im using HTU31D sensor and its working.
Solved! Go to Solution.
2023-08-18 6:59 AM
Hello @Nani96 ,
Did you manage to get a communication with your board?
When you debug your project, where the code hangs/stop?
Maybe need check your device configuration.
It will be better to attach your code and error message, this will help community users to help you.
Imen
2023-08-18 6:59 AM
Hello @Nani96 ,
Did you manage to get a communication with your board?
When you debug your project, where the code hangs/stop?
Maybe need check your device configuration.
It will be better to attach your code and error message, this will help community users to help you.
Imen
2023-11-07 9:03 PM
static void SendTxData(void)
{
uint16_t pressure = 0;
int16_t temperature = 0;
sensor_t sensor_data;
UTIL_TIMER_Time_t nextTxIn = 0;
#ifdef CAYENNE_LPP
uint8_t channel = 0;
#else
uint16_t humidity = 0;
uint32_t i = 0;
int32_t latitude = 0;
int32_t longitude = 0;
uint16_t altitudeGps = 0;
#endif /* CAYENNE_LPP */
// EnvSensors_Read(&sensor_data);
temperature = (SYS_GetTemperatureLevel() >> 8);
pressure = (uint16_t)(sensor_data.pressure * 100 / 10); /* in hPa / 10 */
float Temp = Get_temperature(); // function reads temperature from sensor
AppData.Port = LORAWAN_USER_APP_PORT;
#ifdef CAYENNE_LPP
CayenneLppReset();
CayenneLppAddBarometricPressure(channel++, pressure);
CayenneLppAddTemperature(channel++, temperature);
CayenneLppAddRelativeHumidity(channel++, (uint16_t)(sensor_data.humidity));
if ((LmHandlerParams.ActiveRegion != LORAMAC_REGION_US915) && (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AU915)
&& (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AS923))
{
CayenneLppAddDigitalInput(channel++, GetBatteryLevel());
CayenneLppAddDigitalOutput(channel++, AppLedStateOn);
}
CayenneLppCopy(AppData.Buffer);
AppData.BufferSize = CayenneLppGetSize();
#else /* not CAYENNE_LPP */
humidity = (uint16_t)(sensor_data.humidity * 10); /* in %*10 */
AppData.Buffer[i++] = AppLedStateOn;
AppData.Buffer[i++] = (uint8_t)((pressure >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(pressure & 0xFF);
AppData.Buffer[i++] = (uint8_t)(temperature & 0xFF);
AppData.Buffer[i++] = (uint8_t)((humidity >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(humidity & 0xFF);
if ((LmHandlerParams.ActiveRegion == LORAMAC_REGION_US915) || (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AU915)
|| (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AS923))
{
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
}
else
{
latitude = sensor_data.latitude;
longitude = sensor_data.longitude;
AppData.Buffer[i++] = GetBatteryLevel(); /* 1 (very low) to 254 (fully charged) */
AppData.Buffer[i++] = (uint8_t)((latitude >> 16) & 0xFF);
AppData.Buffer[i++] = (uint8_t)((latitude >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(latitude & 0xFF);
AppData.Buffer[i++] = (uint8_t)((longitude >> 16) & 0xFF);
AppData.Buffer[i++] = (uint8_t)((longitude >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(longitude & 0xFF);
AppData.Buffer[i++] = (uint8_t)((altitudeGps >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(altitudeGps & 0xFF);
}
AppData.BufferSize = i;
#endif /* CAYENNE_LPP */
if (LORAMAC_HANDLER_SUCCESS == LmHandlerSend(&AppData, LORAWAN_DEFAULT_CONFIRMED_MSG_STATE, &nextTxIn, false))
{
APP_LOG(TS_ON, VLEVEL_L, "SEND REQUEST\r\n");
}
else if (nextTxIn > 0)
{
APP_LOG(TS_ON, VLEVEL_L, "Next Tx in : ~%d second(s)\r\n", (nextTxIn / 1000));
}
}
hi, my Get_temperature function always reads 0 if i tried to implement the sensor code in lorawan package.
can any one tell me what was the issue with the code. Im transmitting data in cayenne format.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.