STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CMSIS error "cannot find -llibarm_cortexM7lfdp_math.a"

When I build  my project in "Debug" mode all works fine, if I build the project in "Release" mode an error appears: C:/ST/STM32CubeIDE_2.0.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.20250...

carloV by Associate III
  • 1254 Views
  • 7 replies
  • 0 kudos

MacOS Tahoe can't flash MCU

Hello, I recently switched to a new Macbook os Tahoe. I can't flash MCU. I see some errors pop. CubeMX detects ST link V3 minie, but can't flash it. Same come with the ST link upgrade. The old Mac with the Sequoia can do the job. Any ideas please ?  

Screenshot 2025-12-25 at 22.32.34.png Screenshot 2025-12-25 at 22.33.54.png
grisom13 by Associate III
  • 530 Views
  • 3 replies
  • 0 kudos

Resolved! How to switch a port input<>output on the fly ?

Hi thereI'm a little embarrassed to post this, but..  Coming from Microchip world I would just change TRISx, so simple.As I've learned so far the MX are in charge for setting up a port.But in my application I need to set a 8 bit wide port for paralle...

Baldrick by Associate II
  • 880 Views
  • 6 replies
  • 1 kudos

Resolved! Warning when generate project with LPBAM - Stm32u575

Hi, I am creating application using LPBAM configuration. The application simply is:Enter stop mode 2- Use ADC4-12bit channel 22 (PC4) to measure voltage using clock HSI or MISK- ADC wdog to generate interupt when the value reach threshold to exit sto...

BLS_Karo_0-1766680772291.png BLS_Karo_1-1766680910394.png BLS_Karo_2-1766680952577.png BLS_Karo_3-1766681008354.png
BLS_Karo by Associate II
  • 390 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.