STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Why does the index not work and how to make it work?

In STM32CubeIDE it seems that index don´t work. I tried refresh it, but it didn´t help. This happens when I import existing project into workspace. We tried it on multiple projects and multiple computers, but so far nothing has solved this problem

PŠirů.1 by Associate II
  • 12965 Views
  • 12 replies
  • 1 kudos

Resolved! ADC Triggered by Timer

Hello Team,In my application using STM32G431KCU6 at 160MHz, I want to trigger ADC2 channel by TIM1 channel. I aim to read ADC value synchronously with 1.1kHz pwm signal. When I set up the CubeMX config, i can see that TIM1 trigger OutputCompareCallba...

BKaya_0-1701065655338.png BKaya_1-1701065679267.png BKaya_2-1701065691737.png BKaya_3-1701065745458.png
B.Kaya by Associate III
  • 3721 Views
  • 1 replies
  • 1 kudos

No SDIO option in Cube IDE

HiI am using nucleo-u5a5zj-q board. MCU is stm32u5a5zjt6qu,In cube IDE, i saw SDMMC included but no SDIO driver.May I please know where I could download it?Thanks for the help.

sanfran by Associate II
  • 6326 Views
  • 5 replies
  • 0 kudos

Resolved! CMSIS 5.9 Pack wont install due to errors

Hello Community,I just wanted to install CMSIS Pack 5.9 in my CubeIDE (1.12.1), but the installation is canceled due to errors in the "pack" file:ATM I am using CMSIS 5.7 Pack (Library) but for some reason the >>arm_atan2_f32<< function is missing. S...

cmsis 59.png
CBerg by Senior II
  • 4590 Views
  • 5 replies
  • 1 kudos

Resolved! CAN interface between two STM32F373C8 microcontrollers

Hi, I want to use CAN interface to transfer integer data from one micro controller to another. I am using STM32F373C8 microcontrollers. Please brief me the hardware connection too, from google I understand following.uC1-------------------uC2CAN_H----...

Resolved! Static Code analysis tool for STM32CubeIDE

Can any one suggest ,1. Which static code analysis tool can be used  by STM32CUBE ide?2. The code analysis that is already available in the CubeIDE can be used to generate the Static analysis report?   Thanks in Advance.

Surya S by Associate II
  • 7171 Views
  • 1 replies
  • 0 kudos

Avoid To Include some HAL function of "stm32g0xx_it.c"

Hello everyone!. I'm looking for a way to prevent a function from the "stm32g0xx_it.c" library from being compiled because I'm using it in my MAIN code. The function is "void I2C2_IRQHandler(void)". What I do is to DELETE the function in the library ...

modonga by Associate II
  • 3585 Views
  • 5 replies
  • 0 kudos

Resolved! 1.13.2 problem with List Pinout Compatible MCUs

Hi,if i select in MX "List Pinout Compatible MCUs"i get this:Sometimes STM32CubeIDE closes without warning.i reintalled the ide, i delete the workspace, i restart the pc, nothing helps! i change in the properties from external bowser (chrome) to inte...

padawan_1-1700563206378.png padawan_0-1700563181762.png
padawan by Senior II
  • 4439 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.