STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! ADC Does not work properly

Hello,I'm trying to use the ADC to measure the Vbat voltage on my STM32F401RCT6 but i get some strange values. Here is my setup in the device configuration tool: And here is the code with the returned values: Vref_Val = 303Vbat_Val = 932 I have conne...

Hesseltjuuh_0-1705059418546.png Hesseltjuuh_1-1705059430206.png Hesseltjuuh_3-1705059628054.png Hesseltjuuh_2-1705059475003.png

Resolved! Failed to execute MI command load .elf

Hi everyone! I have a STM32F412RET7 MCU and I made myself a breakout board. However when I try to upload a code I get an error: Failed to execute MI command ... load .elf. This is written in the log file:Log output file: C:\Users\GOSHOA~1\AppData\Loc...

Todoroff by Associate II
  • 8763 Views
  • 9 replies
  • 4 kudos

Still fighting to setup SWO trace on STM32H7

Hello,A few months ago I tried without success to setup ITM on a STM32H753I-EVAL2 board (and STM32CubeIDE). Now I'm trying again. There is a precise point I'm not sure about: the signal SWO is multiplexed on GPIO PB3, so I have to setup PB3 with alte...

Gpeti by Senior II
  • 10185 Views
  • 29 replies
  • 0 kudos

Resolved! STM32Cube Data-Only Project

I'm trying to generate an s-record file that contains nothing but an array of data in flash - no executable code.  (This is used by an external tool and loaded into flash later as config data.)  I deleted everything from the project except main.c.  I...

RHJ by Associate II
  • 2084 Views
  • 3 replies
  • 1 kudos

Resolved! Please login to download a software package

I cannot update my .ioc !Why has this message suddenly appeared?What software package????I've been using Cubeide for years.I have tried logging in etc. etc. as per all the forum posts.I get an OK when I use 'check connection'What is happening to ST?C...

clock1166_0-1704649196921.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.