2024-01-10 7:55 AM
I'm trying to generate an s-record file that contains nothing but an array of data in flash - no executable code. (This is used by an external tool and loaded into flash later as config data.) I deleted everything from the project except main.c. I also stripped everything out of the linker .ld file except the data array. But the compiler still generates a _init and a _fini section of code. How do I get rid of those?
main.c
const unsigned char Data_Arr[] __attribute__((section (".data_arr"))) = /* Test array */
{
0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18
};
.ld file
/* Memories definition */
MEMORY
{
FLASH (rx) : ORIGIN = 0x0801E000, LENGTH = 4K
}
/* Sections */
SECTIONS
{
.data_arr :
{
. = ALIGN(4);
KEEP (*(.data_arr))
} >FLASH
}
List file still contains:
Disassembly of section .init:
0801e000 <_init>:
801e000: b5f8 push {r3, r4, r5, r6, r7, lr}
801e002: bf00 nop
Disassembly of section .fini:
0801e004 <_fini>:
801e004: b5f8 push {r3, r4, r5, r6, r7, lr}
801e006: bf00 nop
S-Record
S010000054657374446174612E73726563FA
S3090801E000F8B500BFA1
S3090801E004F8B500BF9D
S30D0801E00811121314151617185D
S70500000000FA
Thanks for your help.
Solved! Go to Solution.
2024-01-10 11:28 AM
The real data array will be an array of structs about a K long, so it really needs to be compiled with a C compiler.
However, this seemed to work (linker script):
.text (NOLOAD) :
{
*(.init)
*(.fini)
} >FLASH
Thanks again for your help.
2024-01-10 10:42 AM
The compiler/linker is always going to include the c/c++ startup code and other stuff.
How about srecord https://srecord.sourceforge.net/ . You can create a text file with hex values then use srec_cat to create the S-record (or almost any other format) formatted file.
2024-01-10 10:47 AM
Make those "NOLOAD" sections in the Linker Script ?
Making a PC side C app that simply outputs S-Records from an array shouldn't be that hard, format in use since the late 1970's. I've written patching / packaging tools that just natively output .HEX files in Intel, Motorola or Tektronix formats.
As Bob indicates SRECORD is a popular open source version.
I'd suppose OBJCOPY could also be run on a section level basis
2024-01-10 11:28 AM
The real data array will be an array of structs about a K long, so it really needs to be compiled with a C compiler.
However, this seemed to work (linker script):
.text (NOLOAD) :
{
*(.init)
*(.fini)
} >FLASH
Thanks again for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.