STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeMx - ETH Rx Buffers Address no longer there

[EDIT - I had Rx Buffers length before which is still there. I mean Rx Buffers Address which has vanished)Trying to walk the right path to get Ethernet working on a dev board, but using CubeMX as the basis (have looked at LwIP_HTTP_Server_Netconn_RTO...

musmuris_0-1706459004142.png
musmuris by Associate II
  • 6744 Views
  • 3 replies
  • 1 kudos

Resolved! Missing Builder after installing STM32CubeIDE for STM32L5

Hi,I have installed the newest STM32CubeIDE (14.1) and tried to load an example project. Unfortunately, no builder is available. The Project Properties under Builders is just empty.Under Preferences the Toolchain Manager GNU Tools for STM32 (11.3.rel...

MM2 by Associate II
  • 4848 Views
  • 6 replies
  • 1 kudos

Resolved! How do I use a previous embedded package?

I am having trouble with the latest STM32L4 package (V1.18.0) so I wanted to roll back to a previous version.  STM32CubeIDE won't let me change versions, even if I have multiple versions installed and it insists on only using the newest one.  I unins...

JayDev by Senior II
  • 2122 Views
  • 1 replies
  • 0 kudos

Resolved! ST Link Virtual Com Port - USBD_CDC_Init() never called

Hi together,I'm trying to use the ST Link Virtual Com Port on a STM32H745 DISCO board. For this I created a project with the CubeIDE and configured it as explained on many websites and YouTube clips.I also see ST Virtual Com Port in the windows devic...

Download STM32CubeIDE without log in

Hello ST Community,we are building STM32CubeIDE projects with Gitlab CI/CD and a Docker-Image.For this we need the STM32CubeIDE installed in the Docker-Image.The Docker-Image is also built with Gitlab CI/CD.Now we want to download the newest STM32Cub...

rengl by Associate II
  • 5041 Views
  • 4 replies
  • 0 kudos

Resolved! What command is used for flashing the MCU?

From the console of CubeIDE, I have seen that for compiling the command used is make -j9 all. I am wondering what is the command used for running a project given that I cannot see it from the console. 

ubaldot by Senior
  • 1894 Views
  • 2 replies
  • 1 kudos

Resolved! syntax error but no compilation error

hello,I have a syntax error on one line but no compilation error with stm32cubeide 1.14.1HANDLE_busQuadSPI_CREATE(g_hbusQSPI_storage , &g_hqspi) ; //syntax error HANDLE_busSPI_CREATE(g_hbusSPI3_interne , &g_hspi3); // no syntax errorwith#define HAND...

po221 by Senior
  • 11985 Views
  • 19 replies
  • 4 kudos

chinese support in cubeIDE ?

I have been using CubeIDE as a development tool for many years.Compared to KeilMDK, it has a beautiful interface, powerful engineering management capabilities, and many helpful price differences.For example, the ctd completion plugin can greatly impr...

jlinker by Associate
  • 1584 Views
  • 0 replies
  • 0 kudos

Resolved! DAQ System on STM32F103 with fs 100kHz double channel

I need to implement a system with a real and fixed sampling frequency of at least 100kHz, using a STM32F103C8T6, for two analog signals. My main question is: what is the most optimal way to implement this system considering that I also need to do pro...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.