STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! trouble downloading STM32CubeIDE

For the last few days I have tried to download STM32CubeIDE.Often the download page simply ends in an eternal spinner or a page fault.I see others reported the same december 2023 and it appears it just sorted itself.Others see the same now?I have tri...

mogul by Associate
  • 1825 Views
  • 2 replies
  • 1 kudos

LPTIM works at an irregular time delay

I found that LPTIM works at an irregular time delay, it often takes 30-40 seconds to start counting. Also, when l read the current counter, sometimes the LPTIM drops(or l think the counter seems to be restarted) before it reaches the counter period(a...

5c7ea546019783c9b6c8302a9270556.png
ZHANGHN by Associate II
  • 1528 Views
  • 2 replies
  • 0 kudos

Resolved! How to use STM32CubeIDE or STM32CubeMX to automatically add settings for RAM_D2 and RAM_D3 in LD fil

Hi All,Requesting help with below.I am using latest version of STM32CubeIDE. The microcontroller in use is STM32H743BITx.I have concerns with regards to:1. Whether to add ALIGN(4) even inside the FLASH sections present in STM32H753BITX_FLASH.ld (atta...

haw to stm32-mw-openbl

hello to alli want to build project on bluepill board i want to include stm32-mw-openbli got it from https://github.com/STMicroelectronics/stm32-mw-openbl  is there any example for thishaw to include in ide

Elmofty by Associate II
  • 3643 Views
  • 6 replies
  • 1 kudos

STM32F303 debug

Hello, I am working on a project (a custom borad with STM32F303) is it possible to debug it using my nucleo board 32H745 ?The only pinout I did for the MCU is SWD interface with (SWO, SWDIO and SWCLK). I tried connecting pins on the nucleo board in c...

Resolved! How to fix variables to a specific memory using STM32CubeIDE

Hello, everyone.I am using STM32CubeIDE.I want to position one variable in the .noinit section and to secure the memory location of this variable to 0x2001FF0.volatile uint8_t data1 __attribute__ ((section (".noinit")));I succeeded in using the above...

Ekim.1 by Associate II
  • 5937 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.