STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Error building a project cloned with Tortoise SVN

I work on a project that is managed via Tortoise SVN (not sure if it is relevant).On my own machine - I have no problem compiling and building (and of course, debugging).I cloned the repository to a new machine, but I cannot get the code to compile, ...

DBERG.1 by Associate III
  • 2096 Views
  • 3 replies
  • 2 kudos

STM32CubeIDE has no complete compile result

In STM32CubeIDE, in CDT build console, the compile result part, if there are a lot of warnings, only the last part of the compile result can be seen, I have to save the compile log into one file and check from there, it's quite annoying. I think it's...

HXiao.1 by Associate II
  • 3761 Views
  • 7 replies
  • 5 kudos

Resolved! Error in sending message with FDCAN on STM32H735G-DK

Dear all,I've been following this video on YT on how to get the FDCAN on my discovery board (STM32H735G) to work: https://www.youtube.com/watch?v=sY1ie-CnOR0 . Note that this is the 2nd video of a series, if you want to watch it. Now, my problem is n...

Compiler optimized program has errors

While trying to debug a problem, it seems that another one is giving me a hard time.One function call is not shown, another has the wrong name ("writeFLASHDoubleWord" should be "waitForBusy").The breakpoint is also missed. Originally the code worked,...

Tobe by Senior III
  • 29410 Views
  • 37 replies
  • 9 kudos

ADC Returning "0" zeros

Hello. I have a problem with my ADC readings. I use Nucleo 64 with SM32G474 and ADC1 Channel 6. Pin coresponds to A5, Arduino compatible pin on board. No matter what i do, change adc or channel, i get 0 as an output. I use comands MX_GPIO_Init();MX_A...

Miha by Associate II
  • 2230 Views
  • 1 replies
  • 2 kudos

Eigen library and stm32cubeide

I was looking for using the Eigen library with stm32cubeide, but after adding the library, the compiler says it can not find cmath library. I tried to change the project to c++, but the error was persistent. Anyone has any sort of experience?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.