STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Importing drone firmware into STM32CUBEIDE

Not sure if this is the right place to post but for drone firmware such as betaflight or iNav that run off STM32 MCUs like F4xx, how would one go about importing and using the firmware files inside of CUBE IDE so that firmware itself can be changed a...

ZHama.1 by Associate II
  • 5189 Views
  • 4 replies
  • 3 kudos

Using C++ Builder

STMCubeIDE seems to give endless problems. Since the MX can generate c++ code what is the possibility of using all the generated files in C++ Builder? If This is possible, which files should I look for? Has anyone tried this before or will we just ha...

techdesk by Associate III
  • 6634 Views
  • 10 replies
  • 1 kudos

Help Needed: Migrating from MicroXplorer to STM32CubeIDE

Hey everyone,Hope you're all doing well.So, I'm pretty new to ST Microcontrollers and IDEs. I've got a bunch of projects that I've been working on using MicroXplorer. But guess what? MicroXplorer's now outdated. So, I've got to move everything over t...

LuciferD by Associate II
  • 5124 Views
  • 8 replies
  • 3 kudos

Resolved! linker file

The wizard procedure put in my project this file <STM32U575ZITXQ_FLASH.ld> and this file <STM32U575ZITXQ_RAM.ld>.When is used the first and when the second and where is written in the project which one to use?Because in the linker section, as for Deb...

IVent.1 by Senior
  • 4813 Views
  • 1 replies
  • 3 kudos

STM32F4 libusb-win32 with FREERTOS problem

Hello, I'm using STM32F407VGT board to send and receive data to/from a Nodejs application via libusb. This works correctly when not using freeRTOS, but as soon as i create a freeRTOS task or use any CMSIS function such as  osDelay() the board's usb d...

Resolved! stm32f407 ftp client

helloim using stm32f407vgt6 and cubeide without os.i configured ethernet using cubemx perfectly.now i need ftp client, i cant find proper resources for do this.thanks for your helps.

Resolved! Code generation - ADC3 prescaler

In the IDE GUI, when selecting asynchronous clock division for ADC3 on STM32H747XIH, the value generated in the code seems to be taken from ADC1, e.g.:ADC1 (divided by 4):ADC3 (divided by 6):generated code (shortened):/* ADC1 init function */ void MX...

heveskar_0-1713024808318.png heveskar_1-1713024842396.png heveskar_2-1713025453593.png heveskar_3-1713025453592.png

STM32CubeIDE hangs on close

STM32CubeIDE hangs on close, on macbook air mac os Big Sur CPU: Intel core i3. After forced closing, the next time you start STM32CubeIDE, it opens some strange interface that is different from the usual interface (I attach the screen), this problem ...

0693W00000Dn1PqQAJ.png
IAKHM.1 by Associate II
  • 2922 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.