STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

stm32 modbus

I am working on stm32u0 with ultrasonic flow meter, i am facing an issue to receive the response from the device using Modbus communication #include "main.h"#include <stdio.h>#include <string.h>#include <stdint.h> #define PUTCHAR_PROTOTYPE int __io_p...

linker script error in CubeIDE

Error: Cannot find the specified linker script. Check the linker settings in the build configuration.make: *** [makefile:87: fail-specified-linker-script-missing] Error 2 How can I solve this error mesage

Beste by Associate
  • 1568 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer flash works where STM32CubeIDE does'nt

I'm not understanding why ( that why I'm here ...cpt obvious speaking) since 2 days I can't flash or debug under CubeIDE while in the same time connection and flash is working perfectlyfor the record I'm working on a stm32WB35 using a stlink V3 vSTM3...

oga_0-1719329457334.png oga_0-1719319822405.png
oga by Associate III
  • 2206 Views
  • 0 replies
  • 0 kudos

live expressions noticed glitch on displayin values

Hey there. It is quite some time now that I've noticed strange behavior with live expressions. I'm debugging my project in debug optimization "max" and -Og optimization. Debugger that I'm using is "STLINK-V3 compact in-circuit debugger and programmer...

kyf by Associate II
  • 1665 Views
  • 1 replies
  • 0 kudos

Override an autogenerated function in HAL SPI library

Hello everyone,I'm working on a project using STM32 and I'm facing a recurring issue with the STM32CubeIDE and the HAL library concerning the SPI_DMATransmitReceiveCplt() function It is a static function so rewriting it in another source causes error...

eds by Associate III
  • 1482 Views
  • 0 replies
  • 0 kudos

Resolved! stm32f7xx_hal.h: No such file or directory; HAL_Init();

Background:1. STM32CubeMX 6.10.02. Test DMA in UART.3. Using STM32CUBEMX to generate codes.Questions:1. I found the project did not includes source codes.2. The HAL_Init(); is in the main function but it did not have source codes to support.3. I also...

uNavi by Associate II
  • 3267 Views
  • 4 replies
  • 1 kudos

Building Project never finishes

Every time I try to build a project, it says that build has finished but the process never actually finishes it stays at 98%, which prevents me from doing anything else. I have to close cube and re-open it in order to build, it will finish once and t...

RyanSmartIR_0-1718959238773.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.