2024-06-25 12:42 AM
Hello everyone,
I'm working on a project using STM32 and I'm facing a recurring issue with the STM32CubeIDE and the HAL library concerning the SPI_DMATransmitReceiveCplt() function It is a static function so rewriting it in another source causes errors.
In my application, I need to override the SPI_DMATransmitReceiveCplt() function that is auto-generated by STM32CubeIDE as part of the SPI HAL. Every time I regenerate the code from the .ioc file, any custom attributes like __weak are reset, and my overriding function leads to redefinition errors.
Moreover, there is no designated user code section within this specific function where I can safely place my modifications to ensure they remain unaffected by code regeneration.
Here's what I am ideally looking to achieve:
Does anyone have experience with this issue or know of a method to make persistent modifications to auto-generated HAL code in STM32CubeIDE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.