STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Please change GCC stack canary to be weak

Hi Could you please change the library implementations so that  void __stack_chk_fail(void)andunsigned long __stack_chk_guardare defined as weak?I have tested it with GCC 11.3.rel1 and 12.3.rel1 and on both i get "multiple definitions of __stack_chk_...

Resolved! IDE missing SFR DMA TR1

Hi.In SFR Special Funcion Registers view in the IDE some registers are missing. For exampleGPDMA1_Channel4->TR1GPDMA1_Channel5->TR1... 

GDC_0-1718962559684.png
GDC by Associate II
  • 1941 Views
  • 3 replies
  • 0 kudos

Installation of Cube IDE on ubuntu 22.04

hi there,I tried to install latest version of the STM32 Cube IDe 1.15.1 of deb file on Ubuntu 22.4. But it showing me that Segger J-Link is being not downloaded. Any suggestions on how to fix the issue?Below is the errorErrors were encountered while ...

LOW POWER MODE AND SEQUENCER

I AM TRYING TO GET UART DATA FROM A RS485 SENSOR , I AM DOING THIS INSIDE A SEQUENCER , WHERE I HAVE CREATED A SPECIFIC TASK IN WHICH I AM SENDING THE TX DATA FOR GETTING THE SENSOR VALUES , BUT IN SEQUENCER MY CONTROLLER IS RUNNING IN STOP2 MODE , W...

MANOJ_R by Associate II
  • 2493 Views
  • 4 replies
  • 1 kudos

HardFault_Handler

Hi, while doing my project I encounterd some problem.I'm implementing I2C with 1 master and 4 slave boards.Master is NUCLEO-U575ZI-Q and slaves are L432KC.My code is clear. (I'm sure because it works well just few minutes ago..) I debug master to see...

eunni by Associate III
  • 1242 Views
  • 1 replies
  • 0 kudos

Resolved! RTC Timer

Hello everyone,I am using an STM32L152RE board to generate a delay using the RTC as a timer. I would like the onboard LED to blink every 10 seconds. I have tried using a delay via a timer and am now trying to implement the same functionality using th...

Resolved! STM32G0 problem w UART interrupt

Hi,I have a problem with my project. There are two boards MCU1 and MCU2. They are communicating with each other via UART. I simplified program to better understand why it is still not working but somehow I still cant see what the problem. Program des...

Raf_al by Associate III
  • 3119 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.