STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

.ioc nightmare on Linux

Can someone please shed some light on why opening an .ioc file on Linux is like Russian roulette. Sometimes it works, sometimes you get a blank screen, sometimes nothing at all and sometimes 'Yes!!! it's working'.Running IDE 1.16.0 on Linux Mint 21.3...

FFont.2 by Associate II
  • 1890 Views
  • 2 replies
  • 0 kudos

Resolved! Can't override a '__weak' function

Hi,I write my own 'void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)', intend to override the default weak one. But when debug, my version is never called, it always steps into the 'weak' one. I'm new to CubeIDE, the version is 1.16.0, any sugge...

Stm32CubeIde and CMake

Hi!I have started with creating CMake build system for my project. I am using libraries generation in each folder and linking together where needed. Compilation is successfull. The problem is indexer. :Any ideas how to solve this problem without dupl...

Eiffel_0-1721513211067.png
Eiffel by Senior
  • 1156 Views
  • 0 replies
  • 0 kudos

Resolved! debug error with stm32h755 on cube ide

I configured adc+dma of h755 on cubemx and generated code for cube ide.I compile (have not changed the code since it was created) and it's normal.However, when debugging, it runs to this line and cannot exit.H755 board is NUH755ZIQ$AT3, while I debug...

Screenshot 2024-07-19 155024.png
Ruồi by Associate III
  • 3010 Views
  • 4 replies
  • 0 kudos

Resolved! How to input non-numbers in timer configurations?

Hi,In various ST's example .ioc files, the timer PSC, period, etc, are set with text but not numbers. This will define the numbers to macros in the code. But I can't input text in the CubeIDE. So, is this feature only supported in the standalone vers...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.