STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE - debugging startup process

When I start debugging - there is unnecessary focus switching between the startup_stm32f* editor, the focus is constantly broken from the current window and CubeIDE switches the focus to itself - this is strange behavior. Is it possible to remove the...

OlegAjax_0-1723714218174.png
OlegAjax by Associate II
  • 1203 Views
  • 1 replies
  • 0 kudos

Resolved! PWM configuration

Hi, I'm a newbie in this embedded board and I'm having a hard time setting up the PWM pins. I'm currently using an STM32F103RB with a bldc motor driver shield that has pin 5, 6, 9 for PWM input.The corresponding pins for them are PB4, PB10, PC7 so I ...

Issue: No source available for Bootloader

Hello,My project was working fine, but suddenly I cannot debug or run it with the original bootloader anymore. The project is created and generated by TouchGFX Designer.This is the error message I get when I try to debug/run the project.I am sure tha...

mids400_0-1723200878741.png
mids400 by Associate III
  • 2853 Views
  • 4 replies
  • 1 kudos

DS18B20 not registering with internal pullup resistor

I am trying to use the DS18B20 temp sensor on a stm32h7 board to display the current temperature using putty, and if the temp is higher than 45 degrees celsius to display a heat warning, but for whatever reason the sensor is not beign registered. I h...

smakivic by Associate
  • 2200 Views
  • 3 replies
  • 1 kudos

Is there a software update override option?

Hello,I am a Lab Instructor at the University of Waterloo, Ontario Canada.I am using the STM32CubeIDE tools in my lab. There are about 200 students using my lab every term. I have the STM32CubeIDE tools running on 24 workstations in the lab and I hav...

CPope.2 by Associate
  • 2944 Views
  • 3 replies
  • 2 kudos

STM32U0_OTA mode

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body *****************************************************************...

Issue in CAN commnuication with STM32466RE

I am currently working on a project involving two STM32F446RE microcontrollers, each connected to a CJMCU-2551 MCP2551 CAN Protocol Controller High-speed Interface Module. The setup is intended to facilitate CAN communication between the two microcon...

Resolved! RTOS Kernel Awareness don't work

Hello,I’m trying to use the RTOS Kernel Awareness at my FreeRTOS, Makefile Project,but the ROTS Proxy throws following errors:STMicroelectronics RTOS Proxy. Version 0.14.0 Copyright (c) 2023, STMicroelectronics. All rights reserved. Loading RTOS dri...

TWagn.2 by Associate II
  • 4074 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.